Create Your EmojiCube
- Step 1 : 3D print all the components and complete the wiring and assembly steps.
- Step 2 : Connect the first EmojiCube (Node 1) to your PC and upload the sketch for Node1 (Download sketch: EmojiCube_Node1.ino). Make sure the
AVR128DB48
is selected as the tool and the correct COM port is chosen. Verify and upload the code. - Step 3 : Follow step 2 for the second EmojiCube (Node2) and upload the sketch for Node2 (Download sketch: EmojiCube_Node2.ino).
The EmojiCubes should be ready to have some fun with!